• No : 40056
  • Release Date : 2023/08/25 09:04
  • Print

Regarding the QoS function of the MQTT Communication function

What are the different levels of QoS function?
Category : 

Answer

There are three QoS levels and FX5-ENET is also supported.
・QoS0 - The message is sent only once from the source client.
      Messages are not guaranteed to arrive at the destination.
・QoS1 - The message is retransmitted until it reaches the destination client.
       Duplicate messages may arrive at the destination.
・QoS2 - Messages are delivered so that they reach the destination client only once.
       
*The higher the QoS level, the more accurate the message and the higher the quality, but the higher the number of communications, the higher the communication load.
Product Name
FX5-ENET
Product Category
Network/Communication
Series
MELSEC iQ-F Series