Solutions Total Maintenance
In today’s dramatically changing business environment, the impact of
sudden equipment downtime on corporate profits is enormous, and an
increasing number of businesses are implementing planned equipment
maintenance with the aim of achieving non-stop factories.
Meanwhile, the manufacturing industry faces another major issue of
passing down the expertise of highly experienced employees.
Case 11 Monitoring multiple lines from a remote location
Corrective
Maintenance
Line level
When managing multiple lines, it is necessary to switch back and forth between the lines when an error occurs, leading to prolonged downtime.
Remotely monitor of multiple lines
The GOT Mobile function makes it possible to view information collected by GOTs on-site from information devices such as PCs and tablets in remote locations. The operation status, error status, etc. of multiple lines installed at a factory can be monitored remotely without being on site. Users can also use Pocket GOT, a mobile application for GOT, to receive notifications of user alarms that are occurring on monitored GOTs to mobile devices.
The status of the entire factory can be checked at a glance from a remote PC, reducing wasted time when an error occurs, and significantly reducing downtime.