• No : 22110
  • Release Date : 2018/08/27 16:41
  • Print

As to batch storing of data file (EcoWebServerIII).

Any method for collectively store data files stored in the EcoWebServerIII?
Category : 

Answer

Using the setting software attached with an EcoWebServerIII (MES3-255C-EN, MES3-255C-DM-EN), it is able to collectively store data per every kind.
Additionally, it is able to automatically transfer files to the FTP server by means of FTP communication.
Refer to the manual for operation / setting.
The manual is downloaded in this site.
Product Name
Energy Saving Data Collecting Servers
Series
EcoWebServerIII