• No : 22379
  • Release Date : 2018/08/31 14:33
  • Print

Switch disconnector

Answer

Switch disconnector is a switch compatible with IEC 60947-3 standard, and it has no overcurrent tripping element. Please use it as a switch with large switching capacity. The appearance, installation, connection is same as the applicable MCCBs and the same internal accessories can be used.
Product Name
Molded Case Circuit Breakers
Series
WS-V