• No : 22427
  • Release Date : 2018/08/31 14:33
  • Print

CP30-BA micro-load AL/AX

Can CB30-BA AL and AX switch micro-load be provided?
Category : 

Answer

CP30-BA AL and AX switch micro-load can be provided. And the number of installation is same as standard AL and AX switch. However, if multiple AL and AX are installed together, please be careful that the rated value of only AX will be different.
Product Name
Circuit Protectors
Series
CP30-BA