• No : 22432
  • Release Date : 2018/08/31 14:33
  • Print

ACB trip indication

Is there any Trip indication in AE-SW type?
Category : 

Answer

Generally, there is no Mechanical Trip indication of continuous output for AE-SW. It is necessary to indicate electrically by using OCR Alarm (AL) output or Trip indicator (TI). If OCR Alarm (AL) Manual Reset type (MRE:option) is selected, AL signal can be output at the same time as Manual Reset button (front of a circuit breaker) is come out when a circuit breaker trips.
Product Name
Low Voltage Air Circuit Breakers
Series
AE-SW