- No : 22518
- Release Date : 2018/09/03 17:28
-
Print
Difference between Q61P and Q64PN
What are the differences between Q61P and Q64PN?
- Category :
-
Answer
There are differences in 5 VDC rated output current and in 5 VDC overcurrent protection.
The difference in 5 VDC rated output current is as follows.
- Q61P: 6 A
- Q64PN: 8.5 A
The difference in 5 VDC overcurrent protection is as follows.
- Q61P: 6.6 A or more
- Q64PN: 9.9 A or more
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)