- No : 22523
- Release Date : 2018/09/03 17:28
-
Print
Battery life
How long is the battery life installed in a High-Performance model QCPU?
- Category :
-
Answer
It depends on the model of the CPU module, the amount of battery consumption, and the power-on time ratio.
Example) For Q06HCPU with power-on time ratio of 50%, the guaranteed value is 41,785 hours (4.77 years)
For more details, refer to the following manual.
- QCPU User's Manual (Hardware Design, Maintenance and Inspection)
-Appendix 4 Battery Life
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)