• No : 22530
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 14:37
  • Print

CPU modules supporting the serial communication function

Which CPU modules can be communicated via RS-232 interface using the serial communication function from a personal computer,
an Human Machine Interface (HMI), etc.?
Category : 

Answer

CPU modules supporting the serial communication function are as follows.

- Q00UJCPU,Q00UCPU,Q01UCPU
- Q02UCPU 10102 or later (with GX Works2 1.15R or later or GX Developer 8.76E or later)
- Q03UDCPU, Q04UDHCPU, Q06UDHCPU, Q10UDHCPU, Q13UDHCPU, Q20UDHCPU, Q26UDHCPU 13062 or later
   (with GX Works2 1.62Q or later)
 
Product Name
MELSEC-Q Series
Series
CPU