• No : 22541
  • Release Date : 2018/09/03 17:28
  • Print

Online change setting

Is there any case where the online change setting in GX Developer is changed?
Category : 

Answer

Changing to the monitor write mode automatically changes the online change setting in Options to "Write during RUN (while PLC is running)".
With returning to the write mode, the message asking not to write to PLC will appear. Answering Yes changes the setting in Options to "Don't write to PLC".
Answering No keeps the setting "Write during RUN (while PLC is running)" unchanged, and making a conversion in the write mode executes online change.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)