• No : 22567
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 16:48
  • Print

Latch settings

The latch range settings are configured in the device setting of "PLC Parameter".
What are the differences between Latch (1) and Latch (2)?
Category : 

Answer

The setting in Latch (1) can be cleared by latch clear operation.
The setting in Latch (2) cannot be cleared by latch clear operation.
Product Name
MELSEC-Q Series
Series
CPU