• No : 22595
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 17:49
  • Print

PLC write not possible due to memory overload

When I tried to write a comment to the program memory in a High Performance model QCPU, it failed due to memory overload.
What is the remedy?
Category : 

Answer

If comments cannot be stored in the program memory, write them in the standard ROM or a memory card.
Calculate the memory capacity in GX Works2 or GX Developer before performing PLC write to check whether it is possible to write
all data to the program memory.
Product Name
MELSEC-Q Series
Series
CPU