• No : 22600
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 18:52
  • Print

Procedure for developing programs

What should I do in a procedure for developing programs using a C Controller module?
Category : 

Answer

It is necessary to install a development environment (Tornado or Wind River Workbench) and set parameters using the Setting/monitoring tools for the C Controller modules (SW3PVC-CCPU).
Also, debugging requires an Ethernet connection because it is executed from Tornado or Wind River Workbench via the Ethernet connection.
 
Product Name
MELSEC-Q Series
Series
CPU