• No : 22602
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 18:01
  • Print

Boot operation from the standard ROM in the universal model QCPU

Does the universal model QCPU module have standard ROMs, and is it possible to boot from it?
Category : 

Answer

The universal model QCPU modules have their standard ROM but boot operation from the standard ROM is impossible.
Boot the module from a memory card.
Product Name
MELSEC-Q Series
Series
CPU