• No : 22605
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 18:06
  • Print

What to do in the case of the error "A default router IP address needs to be set."

In making the built-in Ethernet port setting for a universal model QCPU module, an error message appears, stating "A default router IP address needs to be set.". Are there any remedies?
Category : 

Answer

When having access bypassing a router, enter only the IP address.The subnet mask pattern is not required to be entered because GX Works2 or GX Developer automatically sets a default subnet mask.

Set the IP address, subnet mask pattern, and default router IP address only when having access via a router.
Product Name
MELSEC-Q Series
Series
CPU