- No : 22635
- Release Date : 2018/09/03 17:29
-
Print
Operation error at the execution of a BIN instruction
Are there any methods of preventing an operation error at the execution of a BIN instruction?
- Category :
-
Answer
Keep SM722 ON or correct the program so that any one of the ten numbers 0 to 9 is stored in each digit of the source data.
An operation error occurs when data other than numbers is stored in each digit of the source data of a BIN instruction.
- Product Name
- MELSEC-Q Series
- Series
- CPU