• No : 22640
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 11:39
  • Print

Making transparent connections using GX Developer

How do I make a transparent connection using GX Developer?
Category : 

Answer

Set as follows in the Transfer Setup window.

 - Select "USB" for "PC side I/F".
 - Select "CPU Module" for "PLC side I/F" and check "via GOT (direct coupled) transparent mode" in the "PLC side I/F Detailed
   Setting of GOT" window.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)