• No : 22641
  • Release Date : 2018/09/03 17:29
  • Print

Whether or not totem pole output type encoders are connected

Is it possible to connect a totem pole output type encoder to the high-speed counter module QD62?
Category : 

Answer

Totem pole output encoders cannot be connected to QD62.
The following types of encoders can be connected.
- Open collector output type encoders
- CMOS level voltage output type encoders
Product Name
MELSEC-Q Series
Series
High Speed Counter Module