- No : 22644
- Release Date : 2018/09/03 17:29
-
Print
Copying programs when replacing the CPU module
Is it possible to copy programs and parameters from the control system CPU module under operation in a Q series redundant system when the standby system CPU module is replaced?
- Category :
-
Answer
Programs and parameters can be copied using the memory copy function.
There are the following two methods of executing the memory copy function.
- Using the memory copy function of GX Developer
- Using special relays and registers
For more details, refer to the following manual.
- QnPRHCPU User's Manual (Redundant System) Section 5.7
- Product Name
- MELSEC-Q Series
- Series
- CPU