FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
>
QCPU built-in Ethernet port setting when using the simple PLC communication function
Back
No : 22654
Release Date : 2018/09/03 17:29
Update : 2018/09/21 12:02
Print
QCPU built-in Ethernet port setting when using the simple PLC communication function
What settings are necessary for the built-in Ethernet port QCPU on the external device side when using the simple PLC communication function?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
Answer
The following settings are required for the "Open Setting" for the number of connected external devices.
- Protocol: "UDP"
- Open System: "MELSOFT connection"
Product Name
MELSEC-Q Series
Series
Q (Q mode)