The communication can be established using the following methods.
- Using the socket communication function of both CPU modules
- Using the simple PLC communication function of the LCPU module
For more details, refer to the following manuals.
- QnUCPU User's Manual (Communication via Built-in Ethernet Port)
Section 7.4 Socket Communication Function Instructions
- MELSEC-L CPU Module User's Manual (Built-In Ethernet Function)
CHAPTER 7 SOCKET COMMUNICATION FUNCTION
CHAPTER 11 SIMPLE PLC COMMUNICATION FUNCTION