• No : 22664
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 13:51
  • Print

Communication between the Ethernet port on the universal model QCPU and the built-in Ethernet port on the LCPU

Is it possible to establish the communication between CPU modules using the Ethernet port on a universal model QCPU module and the built-in Ethernet port on an LCPU module?
Category : 

Answer

The communication can be established using the following methods.
- Using the socket communication function of both CPU modules
- Using the simple PLC communication function of the LCPU module

For more details, refer to the following manuals.
- QnUCPU User's Manual (Communication via Built-in Ethernet Port)
  Section 7.4 Socket Communication Function Instructions

- MELSEC-L CPU Module User's Manual (Built-In Ethernet Function)
  CHAPTER 7 SOCKET COMMUNICATION FUNCTION
  CHAPTER 11 SIMPLE PLC COMMUNICATION FUNCTION
Product Name
MELSEC-Q Series
Series
CPU