• No : 22666
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 13:53
  • Print

Opening a project in an old version of GX Developer

When a project created using the latest version of GX Developer is opened in GX Developer Version 8.58L, the parameters are set back to their default values. Why does this occur?
Category : 

Answer

Products earlier than version 8.58L do not support a project in which the following parameters are set. All the parameters are set to their default values before the project is read.

- Remote I/O
  Projects in which "PLC Operation Mode at H/W Error" is set to "Continue" in the "Intelligent Function Module Detailed Setting
  " window for the I/O assignment setting

- Universal model QCPU modules (Q02U, Q03UD, Q04UDH, Q06UDH)
  Projects in which local devices are set in the "File Usability Setting" window for the program setting
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)