• No : 22667
  • Release Date : 2018/09/03 17:29
  • Print

How to check errors with error codes of QD75

How do I check errors of QD75P1/P2/P4/D1/D2/D4?
Category : 

Answer

Errors can be checked with the following error detection signals and buffer memory areas corresponding to each axis.

- Axis 1 Error detection X8 Buffer memory address 806
- Axis 2 Error detection X9 Buffer memory address 906
- Axis 3 Error detection XA Buffer memory address 1006
- Axis 4 Error detection XB Buffer memory address 1106

The error history allows a user to monitor the last 16 errors using GX Works2 or GX Configurator-QP.
Product Name
MELSEC-Q Series
Series
Positioning Module