• No : 22676
  • Release Date : 2018/09/03 17:29
  • Print

Use of an A-compatible 1E frame for the built-in Ethernet port of the built-in Ethernet port QCPU

An error is returned when I use a command for the A-compatible 1E frame of the MC protocol in a built-in Ethernet port QCPU. Can I use an A-compatible 1E frame?
Category : 

Answer

Check the serial number of the built-in Ethernet port QCPU in use. The Built-in Ethernet port QCPU modules with serial numbers with upper 5 digits of "13102" or later indicate compatibility with the MC protocol's A-compatible 1E frames.
Product Name
MELSEC-Q Series
Series
Q (Q mode)