- No : 22737
- Release Date : 2018/09/03 17:29
- 
          
              Print
          
        
 
Simple PLC communication function
    
      What is the simple PLC communication function?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    This function allows data communications between specified devices at the specified timing, using the built-in Ethernet. 
Device data such as production data can be transferred without a program just by doing simple settings from a programming too. 
Furthermore, this function allows for easy communication not only between the L series devices, but also with existing systems that use the Q series and QnA/A series. The target modules are CPU modules whose first 5 digits of the serial number are "13042" or later.
  
    
      
        - Product Name
- MELSEC-L Series
        - Series
- CPU