- No : 22746
- Release Date : 2018/09/03 17:29
-
Print
Communication between CPUs via built-in Ethernet port in LCPU
Which communication methods are available between CPUs via the built-in Ethernet port in the L series CPU?
- Category :
-
Answer
The following communication methods are available between the built-in Ethernet ports in the L series CPUs.
- Simple PLC communication function
- Socket communication function
- Product Name
- MELSEC-L Series
- Series
- L Series