• No : 22749
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/22 09:12
  • Print

Error code "2200" in LCPU

The error code "2200" is displayed on LCPU. Are there any remedies?
Category : 

Answer

The error code "2200" is "MISSING PARA.".
The causes of the error are described below.
 (1) The necessary parameter file does not exist in all drives.
 (2) When using a parameter file in an SD memory card, the SD memory card is being disabled by SM606
      (SD memory card forced disable instruction).

Refer to the following remedies.
 (1) Write the parameter file to PLC in a desired drive.
 (2) Cancel the SD memory card forced disable instruction.
Product Name
MELSEC-L Series
Series
CPU