• No : 22759
  • Release Date : 2018/09/03 17:30
  • Print

Connection status detection between a hub and the built-in Ethernet port of LCPU

Is there any method to know the connection status between the built-in Ethernet port in the L series CPU and a hub?
Category : 

Answer

The bit 10 of the special register SD1288 provides the connection status to a hub. When the bit 10 of SD1288 is ON, a hub is connected.
Product Name
MELSEC-L Series
Series
L Series