• No : 22785
  • Release Date : 2018/09/03 17:30
  • Print

Simultaneous broadcast transmission setting for built-in Ethernet port LCPU

How do I configure the setting to send simultaneous broadcasts during socket communication of L series CPU with built-in Ethernet port?
Category : 

Answer

To send simultaneous broadcast using UDP, set the parameters as follows.
- Destination IP Address: FF.FF.FF.FFh
- Destination Port Number: Other than FFFFh (Specify the port number dedicated to simultaneous broadcast)
Product Name
MELSEC-L Series
Series
L Series