- No : 22804
- Release Date : 2018/09/03 17:30
-
Print
Difference between standard inputs A06 to B11 and high-speed inputs A12 to B20 of LCPU built-in I/O function
When using the LCPU built-in I/O function, what are differences between connecting to the standard inputs A06 to B11 and to the high-speed inputs A12 to B20 ?
- Category :
-
Answer
The minimum input response times are different. The minimum input response time is 100 microseconds for standard inputs, and 10 microseconds for high-speed inputs, allowing high speed response.
- Product Name
- MELSEC-L Series
- Series
- CPU