- No : 22804
- Release Date : 2018/09/03 17:30
- 
          
              Print
          
        
 
Difference between standard inputs A06 to B11 and high-speed inputs A12 to B20 of LCPU built-in I/O function
    
      When using the LCPU built-in I/O function, what are differences between connecting to the standard inputs A06 to B11 and to the high-speed inputs A12 to B20 ?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The minimum input response times are different. The minimum input response time is 100 microseconds for standard inputs, and 10 microseconds for high-speed inputs, allowing high speed response.
  
    
      
        - Product Name
- MELSEC-L Series
        - Series
- CPU