- No : 22807
- Release Date : 2018/09/03 17:30
-
Print
Remedy for LCPU error "4116"
An error 4116 is displayed on LCPU. Are there any remedies?
- Category :
-
Answer
The LCPU error code 4116 is displayed when a built-in I/O instruction that is disabled in the parameter setting is executed.
Check for the parameter settings and whether or not the built-in I/O function (or instruction) is enabled in the program.
- Product Name
- MELSEC-L Series
- Series
- CPU