• No : 22823
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/27 11:35
  • Print

L60TCRT4(BW) accuracy

What is the accuracy of L60TCRT4(BW)?
Category : 

Answer

- Ambient temperature: 25+/-5 degrees Celsius Full scale x (+/-0.3%)
- Ambient temperature: 0 to 55 degrees Celsius Full scale x (+/-0.7%)
Product Name
MELSEC-L Series
Series
Temperature Control Module