FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-L Series
>
Continuous logging
Back
No : 22829
Release Date : 2018/09/03 17:30
Update : 2018/09/22 15:33
Print
Continuous logging
Is it possible to log 20 samples of analog data at intervals of 0.5 seconds using the LCPU logging function?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-L Series
Answer
Yes.
As a guide, the processing time is shown below.For the logging condition, refer to figure 1 below.
- For 16 devices: 2 ms
- For 64 devices: 6 ms
Product Name
MELSEC-L Series
Series
CPU