• No : 22830
  • Release Date : 2018/09/03 17:30
  • Print

Error code "2110" in LCPU

The error code "2110" has occurred in LCPU. Are there any remedies?
Category : 

Answer

The error code "2110" is "SP.UNIT ERROR.". This error may be caused by one of the following factors.
(1) The module that has been specified by a FROM/TO instruction is not an intelligent function module.
(2) The module that has been specified by a FROM/TO instruction does not have buffer memory.
(3) The intelligent function module that a FROM/TO instruction has specified as an access target is out of order.

The FROM/TO instruction that has caused the error can be specified using the error jump of the diagnostics function (PLC diagnostics) provided by the programming tool, GX Developer or GX Works2.
Product Name
MELSEC-L Series
Series
CPU