• No : 22968
  • Release Date : 2018/09/03 17:31
  • Print

How refresh devices for CC-Link remote inputs and outputs are assigned

How are refresh devices for CC-Link remote inputs and outputs assigned?
Category : 

Answer

The refresh device setting of the CC-Link parameter assigns any devices to the I/O numbers greater than those assigned to the modules on the same base unit. The device set for the refresh device setting of RX/RY is assigned to the first address of station number 1 and the following devices of all other connected modules that are assigned to the successive addresses.
Product Name
Network Related Products
Series
CC-Link