• No : 22979
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/25 17:17
  • Print

Difference between the CC-Link IE Controller Network and a MELSECNET/H network

What are the differences between the CC-Link IE Controller Network and a MELSECNET/H network?
Category : 

Answer

The CC-Link IE Controller Network is an improved system that has a higher processing speed and a larger data capacity than the MELSECNET/H network system (PLC to PLC network).

For detailed comparisons between the CC-Link IE Controller Network and a MELSECNET/H network, refer to the following manual.
 - MELSEC-Q CC-Link IE Controller Network Reference Manual
   Appendix 4 Comparison Between CC-Link IE Controller Network and MELSECNET/H
Product Name
Network Related Products
Series
CC-Link IE Controller Network