• No : 23025
  • Release Date : 2018/09/03 17:31
  • Print

MODE switch setting for QJ61BT11N

What is the use of MODE switch for QJ61BT11N?
Category : 

Answer

The MODE switch can set the following modes.

- 0 to 4: Online mode
- 5 to 9: Line test mode
- A to E: Hardware test mode

Each mode in ascending order of set value provides communication speeds of 156Kbps, 625Kbps, 2.5Mbps, 5Mbps, and 10Mbps respectively.
Product Name
Network Related Products
Series
CC-Link