FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
Network related products
>
CC-Link IE Controller cable standard
Back
No : 23032
Release Date : 2018/09/03 17:31
Update : 2018/09/27 12:14
Print
CC-Link IE Controller cable standard
What are the notes for buying commercial optical cables (type of cable and connector, number of cores, core diameter, cladding diameter, etc.)?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
Network related products
Answer
Use the cables that meet the IEC60793-2-10 Types A1a.1 optical fiber standard. The connectors are LC (duplex) connectors.
Two cores are required.The core diameter is 50 [um] and the cladding diameter is 120 [um].
Product Name
Network Related Products
Series
CC-Link IE Controller Network