FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
Network related products
>
Cascade connections between hubs in the CC-Link IE Field Network
Back
No : 23051
Release Date : 2018/09/03 17:31
Update : 2019/06/27 15:46
Print
Cascade connections between hubs in the CC-Link IE Field Network
Is there a limitation on the number of levels of the cascade connections between hubs?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
Network related products
Answer
UP to 20 levels of cascade connections can be made.
Product Name
Network Related Products
Series
CC-Link IE Field Network