- No : 23052
- Release Date : 2018/09/03 17:31
-
Print
32-bit data assurance
What is the setting required to prevent 32-bit data from being separated in the CC-Link IE Controller Network?
- Category :
-
Answer
To assure 32-bit data, "Network Range Assignment" of the control station must satisfy the following conditions.
(1) The start device No. of LB is a multiple of 20H.
(2) The points assigned per station in LB is a multiple of 20H.
(3) The start device No. of LW is a multiple of 2.
(4) The points assigned per station in LW is a multiple of 2.
- Product Name
- Network Related Products
- Series
- CC-Link IE Controller Network