• No : 23055
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 11:12
  • Print

Precaution about MELSECNET/H connection (1)

What are the precautions for connecting a Q series redundant system using the MELSECNET/H PLC to PLC network system?
Category : 

Answer

 - Set successive station numbers for the network modules in system A and system B in a redundant system.
   (Station number 0 cannot be set.)

 - Match "host's send range" for the network module in system A with that in system B.
   The pairing setting is provided to match "host's send range" for the network modules in system A and B.
   For the control station in a network system including a redundant system, make the pairing setting for the network modules
   in system A and B using the Network Parameter setting.
Product Name
Network Related Products
Series
MELSECNET/H