- Set successive station numbers for the network modules in system A and system B in a redundant system.
(Station number 0 cannot be set.)
- Match "host's send range" for the network module in system A with that in system B.
The pairing setting is provided to match "host's send range" for the network modules in system A and B.
For the control station in a network system including a redundant system, make the pairing setting for the network modules
in system A and B using the Network Parameter setting.