- No : 23172
 
      - Release Date : 2018/09/07 16:09
 
        - 
          
              Print
          
        
 
  
 
The position becomes offset.
    
      •The position becomes offset during automatic drive.
•The position becomes offset after moving the equipment.
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Cause:
- Program error (arithmetic processing, etc.). 
 - Teaching operation error. 
 - Peripheral equipment is offset. 
 - There is a setting error in the origin position data. 
 - The origin position data has been lost(battery life, etc.). 
 - Origin positions are offset(the arm was moved while the power supply was OFF, etc.) 
 - Connecting parts have come loose. 
 - Belt teeth have been skipped. 
 - Increased backlash from the reduction gear. 
 
Measures:
- Check the positioning data in the area where the positioning has become offset. 
 - Check the peripheral equipment and the robot's connecting parts(hand, robot installation section, etc.) 
 - Check the remaining time on the robot battery's life.
 - Check the position of the origin positions.
 - Check the condition of the belt. 
 - Check whether there is any nearby interference, etc.
 
   
    
      
        - Product Name
 
          - Industrial Robots MELFA
 
      
      
        - Series
 
          - FR Series
F Series