- No : 23172
- Release Date : 2018/09/07 16:09
-
Print
The position becomes offset.
•The position becomes offset during automatic drive.
•The position becomes offset after moving the equipment.
- Category :
-
Answer
Cause:
- Program error (arithmetic processing, etc.).
- Teaching operation error.
- Peripheral equipment is offset.
- There is a setting error in the origin position data.
- The origin position data has been lost(battery life, etc.).
- Origin positions are offset(the arm was moved while the power supply was OFF, etc.)
- Connecting parts have come loose.
- Belt teeth have been skipped.
- Increased backlash from the reduction gear.
Measures:
- Check the positioning data in the area where the positioning has become offset.
- Check the peripheral equipment and the robot's connecting parts(hand, robot installation section, etc.)
- Check the remaining time on the robot battery's life.
- Check the position of the origin positions.
- Check the condition of the belt.
- Check whether there is any nearby interference, etc.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series