• No : 23182
  • Release Date : 2018/09/07 16:09
  • Update : 2018/10/03 14:52
  • Print

The operation panel does not light up. Although the T/B has got the electricity, the operation of T/B cannot be done.

•When turning on the power supply of the controller, although the FAN of the controller is operating, the operation panel does not light up the operation of the robot cannot be done.
•Although the T/B has got the electricity, the operation of T/B cannot be done.
Category : 

Answer

Cause:

  • AC line inside the controller may have detected the abnormalities.

 

Measures:

  • Check that the primary side’s power supply voltage is being supplied properly.

 

Product Name
Industrial Robots MELFA
Series
F Series