- No : 23240
- Release Date : 2018/09/12 15:11
-
Print
About Low-voltage Power Distribution Products
How can I select a thermal load relay when it is installed in the deltaphase?
- Category :
-
Answer
When installing a thermal load relay in the delta phase and detectingphase current, you select a heater designation that can be set to 1 / √ 3times of the motor full-load current value and you set the current value ofcurrent knob to 1 / √ 3 times of the motor full-load current value.
- Product Name
- Motor Starters
- Series
- MS-T/N