• No : 23275
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

According to the catalog, the coil designation of S-T and S-N type isAC200V and SD-T, and the coil designation of SD-N is DC100V, buthow about other coil designation?
Category : 

Answer

For other coil designation, it can be calculated as below.1. For S-T* and S-N* type (AC operation type)(1) Input (Instantaneous, constant) power consumption : This value isalmost same as the value described in our catalog.(2) Operating voltage : It is approximate voltage proportion. (When it isAC100V coil, (100/200)* the value described in our catalog)(3) Coil current : Approximately input (instantaneous, constant) / appliedvoltage2. For SD-T* and SD-N* type (DC operation type)(1) Power consumption : This value is almost same as the value describedin our catalog.(2) Operating voltage : It is approximate voltage proportion. (When it isDC24V coil, (24/100)* the value described in our catalog)(3) Coil current : Approximately power consumption / coil voltage(4) Time constant of coil : This value is almost same as the valuedescribed in our catalog.
Product Name
Motor Starters
Series
MS-T/N