• No : 23298
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What is voltage range which can apply to a control coil of SD-Q*type?
Category : 

Answer

At ambient temperature 40℃, the rated voltage (frequency) is applied to acontrol coil, and after temperature rise and saturation, it can operatewithout any trouble at 85 to 120% of the coil rated voltage. Whenapplying the voltage continuously, please use at 95 to 100% of that.
Product Name
Motor Starters
Series
MS-T/N